Other Parts Discussed in Thread: AM3357
From where can i get the serial port numbers of AM335x? ie which port on the board corresponds to ttyO1/ttyO2 etc
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3357
From where can i get the serial port numbers of AM335x? ie which port on the board corresponds to ttyO1/ttyO2 etc
Thanks!
They should correspond, i.e. UART0 =ttyO0, UART1 = ttyO1, etc.
is there a datasheet where i can find which serial port is UART0/UART1 etc? All i see on the board is J10, J11, J12. Do i assume thats UART0/UART1.. ?
One of TI's EVM's or custom board? If it's a custom board you have to check the schematics.
The link isn't opening at the moment but I will have a look at it in a while. I can use the serial ports on the EVM freely right? Do i need to edit the inittab file in /etc or something with sbin/getty?
Thanks!
I cannot say. I'm not a software expert. There are several profiles in which this EVM can be set. Depending on profile chosen the TI distributed Linux EZSDK should configure the board appropriately without attitional intervention.
Hi,
For some reason the link doesnt seem to be working , is there any other documentation?
It's working here, and I work from Bulgaria, outside the TI network. I'm afraid there is no PDF document.
Merging this to the original thread.
I want to use one/all if possible of the serial ports on the daughter board of the AM335x EVM, as well as the LCD display.
HW User Guide is not clear, I assume that I that need to set the CPLD switch for a certain profile? What profile is it and would it allow me to use the UART(s) alongside with ttyO0 UART and LCD? Moreover can i disable the Bluetooth functionality of the J10 UART below the LCD to be used normally?
Thanks
Download the zip file from the link in this paragraph: http://processors.wiki.ti.com/index.php/AM335x_General_Purpose_EVM_HW_User_Guide#Pin_Use_Description
Inside the zip there is an Excel file which contains the peripherals available in each profile.
no profile allows me to get both LCD and additional UART functionalities(apart from UART 0 and BT). Is there any way to get around that?
AM35X SDK 5.07 is no longer available. Only the PSP 04.02.00.07 can be downloaded here: http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/OMAP_04_02/04_02_00_07/index_FDS.html