This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 eMMC boot issue

The boot sequence is [4:0]=11100,MMC1--MMC0--UART0--USB0.

Now SD boots from MMC0 and uart boots are both sucessful. But eMMC from MMC1 fails.

Based on TRM Table 26-29, the pins used on MMC1 boot should be "GPMC_AD0_AD3". But

my  boot pins are "GPMC_AD8-AD11".

Is it OK? Or should I change it to what is described in Table 26-29?

Thanks!