Which versions of openembedded layers will be included in the next MCSDK release? For example the current MCSDK 03.00.04.18 release uses dylan-branch of oe-core. It contains Wayland 1.0.6 whereas the current Wayland version is 1.5. Updating a single component/package to an old oe-core is not a very straight forward thing to do so I was wondering if the upcoming MCSDK release will provide any upgrades to oe-core (and Wayland/Weston specifically)?
regards,
Marko