There is an interrupt being generated at every 10ms on GPIO_39 in the pandaboard OMAP4. I have registered a handler for this in Linux driver code, but the handler is not being called since the interrupt is not being detected.
GPIO 39 is multiplexed to pin 22 of J3 expansion connector. I made sure, by probing pin 22, that the interrupt is being generated every 10ms.
I've the following in my driver code.
iowrite16(0x3, gpio_39_address + 2); /* Configured the pin 22 to be used as gpio. */
#define GPIO_NO 39
ret = gpio_request(GPIO_NO, "Claiming GPIO");
if(ret < 0)
{
printk(KERN_ALERT "%s: Claiming GPIO_%d failed\n", __func__, GPIO_NO);
return -1;
}
else
{
printk(KERN_INFO "%s: Claiming GPIO_%d successful\n", __func__, GPIO_NO);
}
ret = gpio_direction_input(GPIO_NO);
if(ret < 0)
{
printk(KERN_INFO "%s: Setting GPIO direction to input failed\n", __func__);
return -1;
}
else
{
printk(KERN_INFO "%s: Direction of GPIO_%d set to input\n", __func__, GPIO_NO);
}
GPIO_IRQ = gpio_to_irq(GPIO_NO);
if(GPIO_IRQ < 0)
{
printk(KERN_INFO "%s: Mapping GPIO_%d to IRQ failed\n", __func__, GPIO_NO);
return -1;
}
else
{
printk(KERN_INFO "%s: Mapping GPIO_%d to IRQ_%d successful\n", __func__, GPIO_NO, GPIO_IRQ);
}
if((request_irq(GPIO_IRQ, ten_ms_int, IRQF_TRIGGER_FALLING, DEVICE_NAME, NULL)))
{
printk(KERN_ALERT "%s: requeseting GPIO_IRQ %d failed\n", __func__, GPIO_IRQ);
return -1;
}
else
{
printk(KERN_INFO "%s: requesting GPIO_IRQ %d successful\n", __func__, GPIO_IRQ);
}
irqreturn_t ten_ms_int(int irq, void *dev_id)
{
T_UINT32 l;
/* Enable spi channel */
l = ioread32(spi_base + SPI_CHCONF0);
l |= SPI_CHCONF0_FORCE;
iowrite32(l, (spi_base + SPI_CHCONF0));
l = ioread32(spi_base + SPI_CHCTRL0);
l |= SPI_CHCTRL_EN;
iowrite32(l, (spi_base + SPI_CHCTRL0));
/* Enable dma channel 0 */
l = ioread32(sdma_base + SDMA_CCR(CHANNEL0));
l |= SDMA_CCR_ENABLE;
iowrite32(l, sdma_base + SDMA_CCR(CHANNEL0));
/* Enable dma channel 1 */
l = ioread32(sdma_base + SDMA_CCR(CHANNEL1));
l |= SDMA_CCR_ENABLE;
iowrite32(l, sdma_base + SDMA_CCR(CHANNEL1));
printk(KERN_INFO "%s: 10ms interrupt detected %d\n", __func__, irq); /* I know that I've to remove this printk statement */
return IRQ_HANDLED;
}
GPIO_39 belongs to the bank GPIO2 and the corresponding interrupt number is 32. But, the return value of gpio_to_irq() is 199. This is another cause of concern.
Is this the correct way of doing it? Please let me know if something is wrong in the code or if I have missed something. If you need further information, please ask.