whe i create a dsp/bios configure file for my ccs5.5 program.
in the MEM module,there is no CACHE_L2 as in the following figure
i want insert the CACHE_L2 to the MEM ,but there is a erro message as the following figure.
can somebody tell me why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
whe i create a dsp/bios configure file for my ccs5.5 program.
in the MEM module,there is no CACHE_L2 as in the following figure
i want insert the CACHE_L2 to the MEM ,but there is a erro message as the following figure.
can somebody tell me why?
Hi Jack,
Which examples are your trying to run ?
TI examples or own ?
The L2 memory may be configured to run a app.
Please check your linker command ".cmd" file.
Jack,
This question should be posted in the TI-RTOS Forum instead of this C6000 Single Core DSP Forum.
You have allocated the full size of the L2 memory range as IRAM so there is no space remaining for cache.
CACHE_L2 is automatically created by DSP/BIOS based on your configuration settings. Find the location in the configuration settings where you define the size of L2 RAM and L2 cache, and then DSP/BIOS will take care of the allocation for you.
Regards,
RandyP
after creating a "hello world" CCS project ,I Create a DSP/BIOS v5.x Configuration File.
In the MEM, there are only IRAM and SDRAM ,I can‘t find CACHE_L2 in there
After i compile it ,there is no CACHE_L2 in the cmd file or map file.
when i insert the CACHE_L2 ,there is the error message :Object CACHE_L2 already exists!
It is possible that CCSv5 does not create or use the CACHE_L2 section. It is not needed for anything other than preventing you from allocation anything in that same space. You should never use this section, if it does exist, other than to see that it does exist.
The CACHE_L2 section is not needed for proper cache use, only for documentation at the project level.
Regards,
RandyP
Just adding to what the other TI guys have said.
CACHE_L2 is an internal MEM segment created to prevent you from placing any code or data into the part of L2 that is Cache. You cannot create a MEM segment with the same name. You won't see it because you already have the whole L2 RAM segment specified as RAM in your IRAM segment. Hope that makes sense.
Judah
judahvang said:Just adding to what the other TI guys have said.
CACHE_L2 is an internal MEM segment created to prevent you from placing any code or data into the part of L2 that is Cache. You cannot create a MEM segment with the same name. You won't see it because you already have the whole L2 RAM segment specified as RAM in your IRAM segment. Hope that makes sense.
Judah
How can i split some space in the whole L2 RAM as CACHE_L2,and how should i configure the DSP/BIOS?
Yes, its easy to do that. If you right click "Global Settings" and select "properties" and select "64Plus" tab you will see the options to set the size of your caches. So first decided on what cache size you want.
Next if you want to split up the L2 Memory, just modify the base/szie of "IRAM" in MEM by:
Right click "IRAM" and select "Properties". Then change base and/or len and click "OK".
Next Right Click "MEM" and choose "Insert MEM". This will create a new MEM object. YOu can now change the new MEM object with the base and len that you want. Here's a pic of me adding a new MEM0 with base/len.
Judah