Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi,
I want to use ubl copy the U-Boot in OMAPL138.
I only change the DDR2 parameters in OMAP-L138_FlashAndBootUtils_2_40 and compile.
But when I download the sft_OMAPL138_SPI_MEM.bin into SPI Flash.
The UART print as follow:
OMAP-L138 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: SPI
Starting SPI Memory Copy...
No magic number found.
Looking for: 0x55424CBB, but read 0x41504954.
SPI Memory Boot failed.
I don't know much about the UBL and what is magic number ,someone help me?