This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock to UART AM3703

I'm looking at legacy source in an attempt to find the code that controls the clock signal to the internal UART of a 3703.  If I understand correctly, the UART should get 48MHz for proper operation with the OS. And, the clock signal name that drives the UART seems to be CORE_48M_FCLK according to the CPU documentation

Assuming that's the correct signal (is it?) I am unable to locate just how that signal is generated, looking both at my code and the docs.  I am interested in how to get 48MHz here, if the main clock is 19.2MHz.

Any help would be appreciated.

Thanks.