This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet communication

Hi

My goal is Ethernet communication with 2 evm borad each other.I'm using  PA_multicoreExample Project.

and i want to know wich codes should i modify to make my purpose works ??

  • Alaa Darwish,

    The EVM board phy is not configured in the PA_EMAC example, you need to modify.
    Go through the below discussion of E2E post, this will help you,
    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/202083/719489.aspx#719489
    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/146961/690398.aspx#690398
    And also you can try with NDK examples at: C:\ti\mcsdk_x_xx_xx_xx\examples\ndk
    The helloWorld example will run on Core0 only.
    The multicore navigator calls like QMSS, CPPI and RM init calls are done on Core0.

  • Alaa,

    However this discussion of thread can helpful for future readers, If you verified this thread.