This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am using a XTCIEVMK2X board and MCSDK 3.0.4.18. I have set the dip switches for ARM SPI boot and the board is booting from TFTP. How should I modify the U-boot bootcmd script to select Flash boot?
Currently, the bootcmd script is:
boot=ramfs
bootcmd=run init_${boot} get_fdt_${boot} get_mon_${boot} get_kern_${boot} run_mon run_kern
BR
David
Hi David,
David said:How should I modify the U-boot bootcmd script to select Flash boot?
Using setenv and printenv, you can change and view the command scripts on environmental variables. For SPI booting, you can try like below:-
K2HK EVM # setenv bootcmd 'run ${burn_uboot}'
K2HK EVM # saveenv
Use printenv to see the list of varaibles and it's expansion.
K2HK EVM #printenv burn_uboot
Regards,
Shankari
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------
Hi Shankari
After I wrote my last post, your reply appeared. E2E seems to be behaving oddly at the moment.
I understand how to use setenv. What I want to understand is the meaning of the predefined U-boot scripts such as init_ramfs.
BR
David
Hi David,
In your first post you asked for a SPI boot. That's why I have given setting the env for burning uboot into SPI flash.
K2HK EVM # setenv bootcmd 'run ${burn_uboot}'
When you expand the "burn_uboot", you will get like below.
2HK EVM # printenv burn_uboot
burn_uboot=sf probe; sf erase 0 0x100000; sf write ${addr_uboot} 0 ${filesize}
For example, when we want to know about the pre-defined U-boot Scripts, we have to expand and see like below to understand the meaning of them ( init_ramfs, args_all e.t.c).
K2HK EVM # printenv init_ramfs
init_ramfs=run set_fs_none args_all args_ramfs get_fs_ramfs
K2HK EVM # printenv set_fs_none
set_fs_none=setenv addr_uinitrd -
K2HK EVM # printenv args_all
args_all=setenv bootargs console=ttyS0,115200n8 rootwait=1
( Note: Whenever you get a reply to your post, you will immediately get email notification to yourmailbox irrespective of time. By the time, you looked into the post, actually I had deleted and reposted my reply. Hope this clarifies that the E2E doesnot have any problem!.)
Regards,
Shankari.
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------