Hello everyone,
I use customize board, CPU is DM385, firmware is CBB RDK1.5.
I need two kinds of mosaic layout for record and display.
I setup mosaic params [VDIS_DEV_SD] and [VDIS_DEV_DVO2] to same for display.
But only use gVdisModuleContext.swMsId[VDIS_DEV_SD] display size is correct.
like this pic:
If use gVdisModuleContext.swMsId[VDIS_DEV_DVO2], the LCD display size is wrong.
like this pic:
==========================================================================================
usecase link:
cam --> SD Display
merge --> mosaic[ VDIS_DEV_SD] or [VDIS_DEV_DVO2] --> dup -->
cap --> sclr (480x272) --> DVO2 Display
==========================================================================================
I guess somewhere have default settings but I can't find it.
May expert give me some advice for this issue.
Thank you very much.
Have a nice day,
Vic Lin