Other Parts Discussed in Thread: SYSBIOS
Hi,
I've got a Mistral Centaurus Board / VisionMidEve and doing P2P TCP client server communication from a PC via gigabit ethernet. The software is based on the "client" example from NSP.
The software runs on CortexA8 core and when started it prints the following messages:
Negotiated connection: FullDuplex 1000 Mbs
Link Status: 1000Mb/s Full Duplex on PHY 0
Unfortunately the real throughput I've measured with Wireshark is about 70 Mb/s which is 10 times less than I would expect.
Used tool versions:
bios_6_37_02_27
xdctools_3_25_05_94
ndk_2_23_02_03
nsp_gmacsw_4_11_00_00
Board version:
MS_EVE_BB_D_0110
DM814x / AM387x BASE EVM REV D
In addition, please find attached my sysbios configuration.
To me the problems seems to be located in the hardware or driver.
Thanks in advance for any answer.
Kind regards,
Roland