Other Parts Discussed in Thread: AM3359
Hi,
I am interested in adding DMA support in uboot to speed up the booting process.
Before I venture into this project, I have some questions concerning the DMA.
First of all, is the MMC transfer supported by the DMA controller on the AM3359 chip?
If I add the DMA support, what speeds can I expect? (The micron eMMC supports an operating frequency of 52MHz)
Currently, I am getting approximately 9-10 MB/s transfer from the eMMC and SD card.
Side note: It does not matter whether I use the eMMC or the SD card as long as I get a decent performance.