This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3505 ( now AM3505 )

Other Parts Discussed in Thread: AM3517, AM3505

1)       When will we release AM3505 engineering samples ( as opposed to AM3517 )…or will we just have AM3517 for engineering & move direct to fully qualified AM3505 ?

2)       When is the latest schedule date for AM3505 full RTP release ?

3)       Do we have Simple ‘Native’ ARM s/w to exercise RAM, LCD, Ethernet, RTC, SPI, I2C peripherals ??   ie NOT using any O/S……maybe from IAR ??

4)       Has anyone managed to easily make available 20+ GPIO on the AM3517 EVM ?     The problem is that most of the potentially available I/O is already connected to other things on the EVM, and much of it seems inaccessible to the user is they don’t need certain other features.

 Also, do You have a Good LogicPD contact for SoM ????

 ...so I can find out..........

1)       LogicPD plans for a Module with AM3505 specifically ?

2)       Budgetary quote for the above ( expectation is < US$30 )

3)       Could it be made with additional NOR Flash to reduce the Boot Time significantly ?

4)       Is the existing AM3517 SoM orderable via TI, and hence have a DBP for our Disties ??  or must the Customer go direct to LogicPD for Volume SoM ??

5)  Could we request the for CAD files, schematic and pcb, for the Logic SOM Board.....the .pdf on their site is not sufficient.