Hi,
I've create a Project with HTTP server (using tirtos_tivac_2_00_02_36, ndk_2_23_02_03, TM4C129) and i'm trying to send image by calling CGI function without converting the image file with binsrc tool, So what is the suitable HTTP Server exported functions that can be used ? here is my code and it didn't work
httpSendStatusLine(objSocket, HTTP_OK, CONTENT_TYPE_JPG);
httpSendClientStr(objSocket, CRLF);
httpSendFullResponse(objSocket,HTTP_OK, u8fileName);
I used this way because i have a lot of images with big size, so i need to store these file on SD card then send the contents (without using conversion by Binsrc) to save the code size, please tell me if there is another way to handle this problem.
please help me