This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 EVM GEL File Timeout on Startup

I'm dealing with a Lyrtech Dm648 EVM.  When I try to connect to it through CCS after a power cycle the .GEL file hits a timeout during an i2c transfer.  Has anyone else experienced this?  Or does someone have a GEL file that works with this board correctly.  I assume the flakiness on startup probably has to do with poor power sequencing or something along those lines.  Perhaps the MSP430 isn't waiting long enough for 3.3V to stabilize before it enables the power supply for the core.

It seems to behave better if I leave it off for a minute or two when I power cycle.