Other Parts Discussed in Thread: TPS61325
Hi there,
I'm currently using 4AJ.2.5P2 release prebuilt binaries on omap4470 blaze board, when I place CID42_OV5650 binaries under /data/misc/camera/R12_MVEN002_LD2_ND0_IR0_SH0_FL0_SVEN002_DCCID42/ and enabled the few debug prints in hardware/ti/omap44xx/camera/OMXAdapter/OMXDCC.c for readDCC() function I'm able to see this loading and I don't see any error on the ducati logs in
cat /d/remoteproc/remoteproc0/trace1
However when I use the same DCC file for our custom board with OV5650 [ducati is modified for same] I see following error
[ 1.447] [ERR=43] src/config/omx_sup/cam_super_cfg_plugin.c:[108]:[Error] Get Index: 0x7f00005b
[ 1.447] [ERR=44] src/conf_mng.c:[159]:
[ 1.447] Error in src/conf_mng.c, line:159
[ 1.447]
[ 1.447] [ERR=45] omx_rpc/src/omx_rpc_skel.c:[322]:Component returned error: 0x8000100e
[ 1.501] [ERR=46] src/parse_dcc_headers.c:[162]:
[ 1.502] Error in src/parse_dcc_headers.c, line:162
[ 1.502]
[ 1.502] [ERR=47] src/msp_dcc_server.c:[248]:Cannot load specified dcc database!
[ 1.502] Last valid DCC component found 255
[ 1.504] [ERR=48] src/omx_iss_cam_usecase_manager.c:[410]:
I have below questions
1. Can I use the blaze ov5650 DCC files on our custom board as sensor is same.
2. If not what needs to be done ?
3. Do we need to generate the new set of DCC files?
4. Why does the DCC for same sensor does not work if the modification are only in the socket location and i2c of the sensor?
Regards
Anuroop