Hi Experts,
What are the major differences between OMAP4 ISS and OMAP5 ISS ?
Regards,
Gajanan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
What are the major differences between OMAP4 ISS and OMAP5 ISS ?
Regards,
Gajanan
Hi Gajanan,
The major differences between OMAP4 & OMAP5 ISS are:
- OMAP5 ISS is capable of up to 1080p video record at 60 fps with digital zoom, video stabilization, and rotation, while OMAP4 ISS works at 30 fps.
- OMAP5 ISS can 1080p stereo video record at 30 fps with digital zoom, video stabilization, rotation and autoconvergence
- OMAP5 ISS SIMCOP has additional NSF3.0 filter with up to 190 MPix/s throughput at 426Mhz clock speed. Additionally OMAP5 SIMCOP frequencies are incresed:
NSF2.0 provides throughput of up to 127 MPix/s for YUV420 format and up to 85 MPix/s for YUV422 format
Lens distortion correction (LDC) has throughput of up to 213 MPix/s
iMX max clock speed is 426MHz
- OMAP5 ISP has increased pixel throughput of up to 304MHz
Best Regards,
Yordan