This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Align buffer with Cache Line for BCACHE_inv? DM6437



Hello:

In the McBSP driver I noticed that the following call to PAL_osCacheInvalidate() causes the memory BEFORE receiveAddr to be corrupted by data that was previously stored in that memory!

            if( ((Uint32)TrnsAddr %32 != NULL) || ((Uint32)RcvAddr % 32 != NULL) )
            {
                retVal = PSP_E_INVAL_PARAM;
                break;
            }
            /* Move the data to physical memory and invalidate the cache line */

           PAL_osCacheInvalidate(
                        (PAL_osCacheMemAddrSpace)NULL,
                        (Uint32)(((PSP_mcbspTransParam*)(ioHandle->pspRequest.addr))->receiveAddr),
                        (Uint32)(ioHandle->pspRequest.size)
                        );

 That buffer was passed in, and is 32 byte aligned.

I also read this from the DSP/BIOS users guide for BCACHE_inv (Called by PALosCacheInvalidate).

"The blockPtr (start address of range to be invalidated) points to an address in non-cache memory that may be cached in L1P, L1D, L2, or not at all. If the blockPtr does not correspond to the start of a cache line, the start of that cache line is used."

So my question is this.: Am I seeing the problem with alignment to the start of the cache line?  How do I align my buffer to the start of a cache line.  Would this fix this?    Is it sufficient to just align to the largest cache size (L2 = 128 bytes on the DM6437)

Regards,

--B