This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is Max frequency AM1808 support ?

Other Parts Discussed in Thread: OMAP-L138, AM1808

Hello,

We have 2 OMAP-L138 and 1 AM1808 on the same board. So we use the same ARM library for all OMAP-L138 & AM1808.

We're using overclock 456MHz for OMAP-L138 to speed up the DSP process in DSP core, so AM1808 also runs at 456MHz as it shares the same librar

AM1808 appears working, but in some unit it gets hung after some time, few some hours, few some day?

My question is what is maximum frequency AM1808 could run sustainably in a long term ?

Thanks,

~Duy-Ky