This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Data verification failed at address 0x8E000000.Please verity target memory and memory map.

Hello everyone,

I want to flash DM365 through emulator. After I connected the targe board to CCS3.3 by emulator SEED XDS560, and when I load the program "nandwriter_ipnc_dm36x_0.2.0.out",  There is a messagebox posted which showing the error message:

"Data verification failed at address 0x8E000000.

Please verity target memory and memory map."

But, when I do the same operation on another targe board--DM365 IPNC-MT5, there is no error message posted. The only difference between the two targe boards is the DDR2 chip. On the target board DM365, the DDR2 chip is HYB18TC1G160BF-2.5, and on the targe board--DM365 IPNC-MT5, the DDR2 chip is K4T1G164QE-HCE6.

Tthe difference of the DDR2 chips is the key resons for this error??