Hi,
Referring to "Table 2-1. Ball Characteristics" in the datasheet, the gpio_125,126,130,131 are assingned for more than one pin.
For example page 23 says gpio_125's ball location is AA10 and page 23 says it is E25.
But "Table 2-2. Multiplexing Characteristics" mentions that this pin(gpio_125) is assigned only for AA10.
Which of the tables are correct?
Kindly let me know if this is a typo or if this has some other feature.
Thankyou in advance.