This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it OK to use the same boot loader for both AM1808 & OMAP-L138

Other Parts Discussed in Thread: AM1808, OMAP-L138, OMAPL138

Hello,

We have one AM1808 and two OMAP-L138 on the same board and all are running at 456 MHz.

We are using the same boot loader for all of them for more than a years of development and have not seen any problem.

We're about to release a new product using this board and I like to make sure every is NOT out of tech specs

I just to check with TI tech guys that that approach is OK within the technical usage of these MCU's

Thanks,

~Duy-Ky