This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help on PMIC and battery capacity - EPOS reference design

Other Parts Discussed in Thread: TPS65910A, AM3352, AM3359

Hi All,

I want to design EPOS based on already existing ready solution from TI. I checked completely the details, i am not able to find the battery current capacity & battery part number of 7.4V & 3.4V batteries used in the design, pl let me know from where i can get it.

As i am planning to use 9V adaptor, do we have any PMIC for AM3352 with input voltage of 10V, i checked with TPS65910A but it is having only 5.5V.

Kindly help me on the same 

Regards,

Aravind