Hi everyone,
I want to specify the video output position on the screen and the window size, how can I implement it? My platform is angstrom omap3530bealge, I use gstreamer-ti play video and output to TIDmaiVideoSink Thanks !
Best Regards,
Carl
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
I want to specify the video output position on the screen and the window size, how can I implement it? My platform is angstrom omap3530bealge, I use gstreamer-ti play video and output to TIDmaiVideoSink Thanks !
Best Regards,
Carl
Hi Carl,
TIDmaiVideoSink does not support setting a position for the video, only the size (VGA, 480P, etc.) You can set the position using the DSS2 interface, which is documented here:
http://wiki.davincidsp.com/index.php/OMAP3_DSS2_Architecture
However, I suspect that TIDmaiVideoSink will likely overwrite anything you set up through DSS2 so some customization of TIDmaiVideoSink might be required to prevent that.
Regards, Clay
Hi,
You can take a look at the TIDmaiVideoSink on DDOMPE's branch, it already have code to set the X and Y position (and a lot of other changes, so you will have to cherry pick what you are looking for)
Diego
Hi Clay && ddompe
Thanks for your reply! I modify the position by an easy way: just change the value of the overlay's output position:
cd /sys/device/playform/omapdss/overlay1
echo x,y >position
This will change the video position on the screen.
BestRegards,
Carl
Hi ,
I can adjust the video output position on the screen now, but how can I implement the video resize? I check the code of gsttidmaivideosink.c, and modified the code in function:
gst_tidmaivideosink_init_env:
if (gst_ti_env_is_defined("GST_TI_TIDmaiVideoSink_resizer")) {
sink->resizer = gst_ti_env_get_boolean("GST_TI_TIDmaiVideoSink_resizer");
printf("Setting resizer=%s\n",sink->resizer ? "TRUE" : "FALSE");
}
// I added the following line to set resizer enable followed above code(about line:373 in file gsttidmaivideosink.c).
sink->resizer = 1; // added by carl
then, when function: gst_tidmaivideosink_render was called, it print: Unable to initialize display, it's due to the failure of gst_tidmaivideosink_init_display,
then i check gst_tidmaivideosink_init_display, this function failed when call : Resize_create, and print: Failed to create resizer. I check code Resize_create
and found it will open device: /dev/omap-resizer, but I found there's no such file on my device ! What's the reason ? Could you give me some suggestion ?
My platform is beagleboard omap3530.