This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current in GPIO pins EVM5515

Hi,

I would like to know which current can provide GPIO pins and if it is configurable. I have connected a LED between GPIO4 and GND. The idea is to turn the LED ON by setting GPIO4 as output and set it to high level.

The LED I've used turns on when the voltaje is over 1.7V. However, i can't turn it on when the VDD_IO1 is set to 1.8V. I measured the voltaje with an osciloscope and the voltaje is about 1.72V. Then i tried the same by setting the VDD_IO1 to 3.3V and the Led turns on but it makes very por luminosity. I tried this LED with a power source and it has a high luminosity with 2mA.

I think that GPIO provides very low current. Can anybody show me?

Thanks in advanced!