Other Parts Discussed in Thread: TPS65910
Hello World!
My RTC is running a few second slow each hour, could some one please explain why and how to tweak any S/W or H/W parameter to compensate/calibrate this drift timer?
My Linux timer is running slower also, but I know I can adjust that with cron job on adjtimex, etc... but I understand that the hwclock need to be fixed with kernel RTC tweak ??
Here is the dmesg clock, if that help. Thanks!
root@amadel:/>dmesg|grep clock
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.135742] Switching to clocksource gp timer
[ 2.244750] clock: disabling unused clocks to save power
[ 2.265472] tps65910-rtc tps65910-rtc: setting system clock to 2000-01-01 22:05:33 UTC (946764333)