This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Yocto SDK6 fail to build on Ubuntu 14.04



Ubuntu 13.04 repo has been officially removed. Therefore, I upgrade my computer to Ubuntu 14.04 LTS and re-build my meta-layer for AM335x.

I found only Yocto version 1.6 supports Ubuntu 14.04 LTS. TI SDK6 is based on Yocto 1.5 and it fails to build. The error messages are

tar: --same-order option cannot be used with -c
    Try 'tar --help' or 'tar --usage' for more information.
    tar: This does not look like a tar archive
    tar: Exiting with failure status due to previous errors

The issue comes up if user's distro is using GNU tar version 1.27 which is a standard package in Ubuntu 14.04 LTS.

root@dns3:~# tar --version
tar (GNU tar) 1.27.1
Copyright (C) 2013 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>.
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.

I believed that more and more people will upgrade to Ubuntu 14.04 LTS because 13.04 is no longer supported.

What is the best way that TI suggests to work around this??

-Eric