This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 USB bulk device driver for win8



Hi,

I 'm using a C6748 custom board and using USB for communication, and the PC need stall usb driver, but i find the link http://www.ti.com/tool/sw-usb-windrivers, and find the drivers just for winXP and win7, but my pc is win8.1, so i need the drivers for win8, where can i download the driver, or anyone who can provide.

  • Hi Jie,

    In title, you have mentioned "C6748 USB bulk device driver for win8",

    What bulk device driver you need ?

    Do you want USB driver to work with CCS and emulator or something else ?

    Could you elaborate bit on your requirement ?

  • I wait my custom board to communicte with PC(the OS is Windows 8.1 professional vision) using USB, the PC is host, and my board is using as device, so the PC should install a driver. in the ti web, i just find the windows usb drivers provided for Windows XP and Windows 7, not for windows 8, so my PC(The OS is windows 8) cannot recognize my board, So i need a windows usb driver for win8.

  • Hi Jie li74477,

    The device side USB bulk driver for C6748 will be found as a part of C6748 starterware package.

    The host side driver for Windows 8 must be a generic/common driver which supports all the USB bulk devices.

    I guess, You have to google and find the driver for Bulk USB devices for Windows 8 as it will be maintained by Windows.

     

    Regards,

    Shankari

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------