This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 Errors in DVTEvent_Log

Hello:

I enabled EDMA3 instrumentation by defining...

        EDMA3_INSTRUMENTATION_ENABLED

And I now see the following ERRORs (below).    What are they?  What does this mean.  Where are they logged from?

The EDMA3 code seems to always start the log message with EDMA3.  Note that these ***ERROR do not start with EDMA.

I saw a similar problem with McBSP instrumentation.

Regards,

--B

 

 

0 EDMA3

0 *** ERROR: 0x7 0x7274e50 ***

0 *** ERROR: 0x6 0x7275227 ***

0 *** ERROR: 0x6 0x727544c ***

0 *** ERROR: 0x1 0x7273e99 ***

0 *** ERROR: 0x1 0x7273f41 ***

0 *** ERROR: 0x1 0x7274152 ***

0 *** ERROR: 0x1d00000 0x72713bb ***

0 *** ERROR: 0x1d00000 0x72708f5 ***

(MORE ERRORS not included here)

1 EDMA3

2 EDMA3

3 EDMA3