This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Run different codec on C6678 DSP card simultaneously



Hi TI expert,

Is it possible to run different codec on C6678 DSP card simultaneously?

ex:

I. DSPC8682 card multichip application -  run H264 codec on DSP0-2, run H265 codec on DSP3-7

II. DSPC8682 card multicore application - run H264 codec on Core0-2, run H265 codec on Core3-7

III. DSPC8682 card - download sv04.out on DSP and pass different channel parameter to select the specific codec 

for example:the first frame is processed by H265Enc, so pass the parameter「--channel="H265 Encode"」, the second frame is processed by H264Enc, so pass the parameter「--channel="H264HP Encode"」

  • Hi,

      Can you check the H264 Multi Channel demos under: mcsdk_video_2_2_0_41\demos\codecs\pcie_h264hpenc_multichan_demo\scripts

    This example is for Running multiple H264 codecs, the same you can modify it for running other multiple codecs. I could not understand the example given.

  • Hi Prasanna

    1. Is it possible that  decode H264 data on DSP0-2 and then pass the data to encode H265 on DSP3-7 ?

    -> Is this similar to 1080p_h264dec_scale_720p_h265enc demo?

    2. Is it possible that  decode H264 data on Core0-2 and then pass the data to encode H265 on Core3-7 ?

    ->Is this similar to 1080p_h264dec_scale_720p_h265enc demo?

    3. I mean that can I pass the different channel parameter at the same time to select the specific codec since TI various codec are all in sv04.out

     

    Regards,

    YC

  • Hi YC, yes please use 1080p_h264dec_scale_720p_h265enc demo as an example demo for your use case (decode H264 data on DSP0-2 and then pass the data to encode H265 on DSP3-7)

    thank you,

    Paula