Other Parts Discussed in Thread: TVP7002
Hi,
I am using DM816x with EZSDK 5.05.02.00, we are planning to capture several resolutions using the VIP0, looking into the documentation and other posts I found that the VPSS driver can capture until 1920x1200 with the correct reduce VESA blanking, however, it is not mentioned a list of resolutions supported in that range, we are planning to support:
640 x 480 60 Hz 25.175 MHz
800 x 600 60 Hz 40.000 MHz
848 x 480 60 Hz 33.750 MHz
1024 x 768 60 Hz 65.000 MHz
1280 x 768 60 Hz 68.250 MHz
1280 x 800 60 Hz 71.000 MHz
1280 x 960 60 Hz 108.000 MHz
1280 x 1024 60 Hz 108.000 MHz
1360 x 768 60 Hz 85.500 MHz
1400 x 1050 60 Hz 101.000 MHz
1440 x 900 60 Hz 88.750 MHz
1600 x 900 60 Hz 97.750 MHz
1600 x 1200 60 Hz 162.000 MHz
1680 x 1050 60 Hz 119.000 MHz
1920 x 1080 60 Hz 148.500 MHz
1920 x 1200 60 Hz 154.000 MHz
Do you know if these resolutions are supported by the VPSS driver? I know that V4L2 will need to be extended to support these resolutions.
Thanks for your help,
-David