Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Please help with following three questions of using SDRAM under EMIFA interface in OMAP-L138 chip:
- From the 1st page of OMAP-L138 spec under the "Two External Interfaces/EMIFA" section, it stated 16-Bit SDRAM with 128MB address space. However, in Table 6-18, it shows the max SDRAM goes up to 512MB (with two SDRAM loads). Why the discrepency (128MB vs 512MB)? Is it because 512MB can only be allowed if freq scale down to 100Mhz??
- Is SDRAM operating at 3.3v range only? Can it run at 1.8v? Looking at all its control lines from spec, it's can be powered from either 3.3v or 1.8v.
- In the case where one needs to put two external SDRAM (both at 256MB) to reach 512MB, does it affect the multiplexing feature of the chip where some control needs to be setup properly in order for two chips to work at the same time? If so, where in the spec does it mention this?
Thanks! Stephen