Hi,
i would like to use device tree overlays on BBB and therefor i need the compiler. I downloaded the sdk7 and tried to follow the instuctions here: http://processors.wiki.ti.com/index.php/WL18xx_AMxxx_platform_integration_guide
I downloaded the pre-compiled image for beagle bone black:
| June 20, 2014 | SDK 7.0 | am335x-bone(black/white), am335 EVM | boot partition, rootfs partition | Includes SS1 bluetooth stack v4.0.1.4.2 binaries in /home/root/ss1 |
and used the create_sdcard script of the sdk 7 to flash a sd card.
after i established a serial connection, i tried to use the command: dtc -O dtb -o .... to compile files but the command doesn't exist:
dtc: command not found
Does this image doesn't have this function or do i have to create the image like explained in the upper link on a built server to make the compiler work?
Maybe you can point me in the right direction
thanks
Beni