Other Parts Discussed in Thread: AM3354, TPS65910A
We are involved in designing a system with the AM3354 as processor. I have a few doubts regarding the schematic design provided by TI and the data sheets. It would be of great help if someone could clarify the following for me.
1. The PMIC TPS65910A3 has its RTC output given as VPMIC_VRTC. Why is there an LDO TPS71718 (U5) with a VRTC output then? Can't we use the VRTC_PMIC so that the PMIC is the single power on and power control chip ?
2. Even if an external LDO U5 is to be used, VRTC should be connected to U26C.D6 (CAP_VDD_RTC) and not U26C.D7(VDDS_RTC). Also it should be 1.1V and not 1.8V?
Also, the first design that we made uses an earlier revision of the AM335X. We want to use silicon revision 2.0 or above for our next design onwards. The Schematics and PCB for this is not yet available. When will this be reaady?
Thanks..:)