This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP35x] MMC1 3v GPIO???

 

I found this wiki post very interesting:

http://tiexpressdsp.com/index.php/Additional_Configuration_for_GPIO120-129_on_OMAP35x

My question is if I configure MMC1 as 4 bit SD (3v) can I use GPIO 126-129 as GPIO i.e. Input and Output?

If so does this mean if I set the PBIAS register correctly for these bits I can actually get 4 bits of 3v tolerent GPIO?

If so what would be the GPIO output voltage swing? What would be the input voltage tolerence? Can I actually use these bits to interface to a 3.3 volt peripheral?