Hi,
I have started using sdk version 07 with linux kernel 3.12 (from the board-port git repository). Everything so far is working fine except for the touch interface. It seems that after the first touch event there starts a flood of touch events. As an example the output of ts_print:
# ts_print 96.162276: 297 281 137 96.164141: 645 192 216 96.166009: 779 176 247 96.166009: 779 176 247 96.167878: 780 176 247 96.169742: 779 175 247 96.171606: 779 175 247 96.175334: 473 283 188 96.177198: 312 302 162 96.179060: 304 304 163 96.179060: 301 304 164 96.180924: 301 304 165 96.182788: 298 305 169 96.184652: 298 304 173 96.186515: 298 304 177 96.188378: 298 304 181 96.190244: 298 304 184 96.192108: 298 304 185 96.193971: 298 304 187 96.195834: 298 304 188 96.197698: 298 304 188 96.199561: 298 303 188 96.201425: 299 303 186 96.203289: 299 303 183 96.205152: 299 303 178 96.207015: 300 303 173 96.208879: 300 303 171 96.210745: 301 304 168 96.212608: 301 303 167 96.214471: 301 303 167 96.218198: 320 284 142 96.220064: 626 196 212 96.221927: 779 175 247 96.221927: 779 175 247 96.223790: 779 175 247 96.225654: 779 175 247 96.227517: 779 175 247 96.229381: 778 175 247 96.231245: 778 175 247 96.233108: 777 175 247 96.234971: 778 175 247 96.236835: 778 175 247 96.240555: 778 175 247 96.242418: 778 176 247 96.244281: 778 175 247 96.246144: 778 175 247 96.248008: 778 175 247 96.249872: 779 175 247 96.251735: 778 175 247 96.253599: 778 175 247 96.255462: 779 175 247 96.257326: 779 175 247 96.259189: 779 175 247 96.261055: 778 175 247 96.262918: 778 175 247 96.264782: 778 175 247 96.266645: 778 175 247 96.268508: 778 175 247 96.270374: 779 175 247 96.272238: 779 175 247 96.274101: 779 175 247 96.275965: 779 175 247 96.277828: 779 176 247 96.279692: 779 176 247 96.281555: 779 176 247 96.283420: 779 176 247 96.285284: 779 175 247 96.287147: 779 175 247 96.289011: 779 175 247 96.290874: 779 175 247 96.292737: 780 175 247 96.294601: 779 176 247 96.296464: 779 176 247 96.298328: 779 175 247 96.300194: 779 176 247 96.302057: 780 175 247 96.303921: 779 175 247 96.305784: 779 175 247 96.307647: 779 175 247 96.309510: 778 176 247 96.311374: 779 175 247 96.313238: 779 176 247 ....
After starting ts_print there is no output but after the slightest touch of the panel, the flood of output starts and will not stop anymore.
Are there any hints, what could be the cause for this? On kernel 3.2 the touch is working fine.
cheers