This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365: jpeg encoder with extender parameters



Hello,

I'm trying to create a jpeg encoder using dvsdk_2_10_00_17 and dm365_codecs_01_00_06 within DMAI. I can't make it work if I try to use extended parameters, the call to Ienc1_create crashes. This is the structure I am using:

width=704; height=480;

IJPEGENC_DynamicParams IJPEGENC_DynamicParamsExt;
IJPEGENC_DynamicParamsExt.imgencDynamicParams = Ienc1_DynamicParams_DEFAULT;
// IJPEGENC_DynamicParamsExt.imgencDynamicParams.size = sizeof(IJPEGENC_DynamicParams); <--------------- IF COMMENTED, IT WORKS
IJPEGENC_DynamicParamsExt.imgencDynamicParams.numAU = XDM_DEFAULT;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.inputChromaFormat = XDM_YUV_420P;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.inputWidth = width;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.inputHeight = height;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.captureWidth = 0;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.generateHeader = XDM_ENCODE_AU;
IJPEGENC_DynamicParamsExt.imgencDynamicParams.qValue = 50;
IJPEGENC_DynamicParamsExt.rstInterval = 84;
IJPEGENC_DynamicParamsExt.disableEOI = XDM_DEFAULT;
IJPEGENC_DynamicParamsExt.rotation = 0;
IJPEGENC_DynamicParamsExt.customQ = NULL;

Basically if I comment the line setting the size to the extended version, Ienc1_create works without problems (using only "basic" parameters). If I uncomment the line, the size is set for extended version of the structure and all the last 4 parameters are considered. In this case, the call to Ienc1_create crashes.

If I execute the app with "DMAI_DEBUG=2", this is the output of the Ienc1_create call.

@0x005b033a:[T:0x438a2490] ti.sdo.dmai - [Ienc1] XDM_GETBUFINFO failed, status=-1

So it seems in my case that using extended version of the dynamic parameters, encoder creation does not work. Basic parameter values are the same.
Any idea?