This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

K9F1208U0C using with DM355EVM?

Hi

I am using DM355EVM,but need change nand flash to K9F1208U0C,it look like not work in DM355EVM.

I see leopard is use the same chip,is the UBL or SFH need modify or some place need change??

I use DM35x_FlashAndBootUtils_1_50 to download program into nand flash.

Thanks