Hello All,
I am having trouble figuring out how to assign IRQ2 to GPIO3_17 in my DTS file as a shared low level interrupt. Our hardware is basically a BeagleBoneBlack with an external DUART attached that will be using GPIO3_17 as its interrupt signal to the processor. Could anyone point me in the right direction or share any sample code that I can use as a reference? We are using kernel version 3.12.
Thanks in advance for any help - Anthony