I am using the LogicPD EVM board(s) with the TMS320C6748 SOM. I understand that there is a 10-bit, 20 M sample/Second A-to-D converter on-board somewhere. I presume it is connected to the SMA connector labeled "connector H" on their Quick Start Guide. ??? Am I right?
I need to DMA data from the A-to-D converter into memory at a high rate of speed. So I am looking for info on how to do that. I suspect there is already a test program available (in the bundle that came from LogicPD). Such as their program test_cvideo or test_svideo. ??? I dunno.
Can you steer me toward the information I need?
[Note: By the way, my board differs from the photo given on page 8 of their Quick Start Guide 1014618rev4_OMAP-L138_EVM_QSG.pdf. That is, on my board the connectors G & H are swapped -- And on my board the connectors C & D are swapped -- compared to their diagram. I presume this is no big deal, as I am able to identify the connectors by eye.]
Thanks for your help.