This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 resizer hang

Hi all,

   We have met a problem.

   My program is based on IPNC_RDK_3.5.0.

   Iif it runs over 12~24 hour, the resize stop trigger interrupt,   sometimes it will print

   "m3vpss ]      ##################### REISZER OVERFLOW OCCURED:                      RESTARTING...############################" and some times not.

Our use case is something like the following:

sensor->RSZA------------------------------------------------}

                RSZB->dup---->1920x1080------- ------------}->merge->encode->
                             |-->SCALAR->352x288 ---------------}
                             |-->SCALAR->720x576

(D1 for tv out, cloesed to decrease the bandwidth in normal time, open when needed) 
We didn't use the H3A on chip.

camera and resize resolution:

sensor(or camera) 2336x1760(YUV422)  25fps
RSZA                         2592x2048                    25fps
RSZB                         1920x1080                    25fps

SCALAR1                 352x288                         25fps

encode resolution:

 2592x2048(JPEG,5fps)
1920x1080(H264,25fps)
352x288(H264,25fps)

DSP: customized algorithm for vehicle recognition.

The frequency of our customized board:

L3 clk : 220MHz
IVA clk : 450MHz
ISS clk : 560MHz
DSP clk : 750MHz
DSS clk : 200MHz
ARM clk : 1000MHz
DDR clk : 533MHz

The configure of DDR controller:

total 1G bytes.

EMIF0 and EMIF 1 each has 2 16bit ddr chips.

LISA MAP :128byte interleaved.

We have noticed and read the following thread:

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/265001.aspx?pi199607=1
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/242555/851247.aspx#851247
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/163881/604055.aspx#604055
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/323639/1130127.aspx#1130127

and downloaded  and compiled the code of new sys_pri.zip.

We have modified the script in init.sh as following:

./bin/sys_pri.out --L3-bw-reg-set HDVICP0 0 0 900 2500&
./bin/sys_pri.out --L3-bw-reg-set ISS 3 3 700 2500&
./bin/sys_pri.out --dmm-pri-set ISS 0&
./bin/sys_pri.out --dmm-pri-set HDVICP0 1&

(It seems that only HDVICP0, ISS, SGX can use --L3-bw-reg-set option, other ID will cause a bus error)

We tried the following values of PBBPR:

0xFFFFFF
0xFFFF20
0xFFFF10
0x90FF30

and tried the flollowing the clock divider values:

a.
ispPrm.clkDivM = 14;
ispPrm.clkDivN = 30;

b.
ispPrm.clkDivM = 10;
ispPrm.clkDivN = 20;

the option we have not tried:

add the vertical blanking line of sensor.

The result of test:

We have not fount a perfect solution of resize hang.

Some times our application can run over 3 days(we have three test equipment), but next time after re-power up, some of them(random) can run only 12 hours~24 hours.

this problem has confused us for a long time.

Please give me some clues for next test.

Thanks a lot.