So my input is a real sine wave with a period of ~60 points, and therefore a 512 or 1024-point cfft_SCALE function should give only one peak (or two, if consider the symmetry). However, there are peaks at multiples of 2 (16, 32 64 and 128, etc), and does anyone know how they are generated?