This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All i issued a booting problem using SDK v07.00,
i use custom board you can find schematics here :
https://www.olimex.com/Products/SOM/AM3352/AM3352-SOM/resources/AM3352-SOM_schematic.pdf
Here is boot log :
http://pastebin.com/fHcDSd9m
and dts file :
http://pastebin.com/fwpQPkKv
Kernel is built using default am335x config, and mmc driver is enabled and built in
Thanks for your help in advance!
~Best
Hi Dimitar,
Can you describe what the problem is?
Hi,
What is the filesystem you are using on the root partition of your SD card? Check whether you have kernel support enabled for the particular file system.
Best regards,
Miroslav
Hi Miroslav,
i use ext4 FS , and yes ext4 is built into kernel.
grep EXT4 .config
CONFIG_EXT4_FS=y
u-boot environment is default, so i think this is mmc driver SD Card detection bug.
When i try to list sd contents in u-boot it works fine . I can see files and partitions.
~Best
Dimitar, I can't see the pinmuxing for the MMC pins in your .dts file. Did you do it inside am33xx.dtsi?
Best regards,
Miroslav
I can see you are using the MMC controller's SDCD pin. Please try using a GPIO and specify the GPIO pin inside the .dts file using:
cd-gpios = <&gpio ## #>;
More information inside <linux_kernel_dir>/Documentation/devicetree/bindings/mmc/mmc.txt
Best regards,
Miroslav
Hi Miroslav,
i just made changes you talking about.
I add following lines to my dts file :
mmc cd pin :
mmc1_pins: pinmux_mmc1_pins {
pinctrl-single,pins = <
0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
and
&mmc1 {
status = "okay";
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc1_pins>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
};
This cause kernel panic @omap4_rng_init
Please see log here :
http://pastebin.com/gySYTZdn
Best Regards,
Dimtiar
Try to disable the random number generator for now, in order to at least see if the MMC card would be successfully detected by the kernel.
Best regards,
Miroslav
When Random HWGen is disabled board boots and hangs at same place.
I made some tests with 3.11.0 and board boots fine. So i think this must be some kernel config problem. When I run diff on configs there is no significant difference.
So i am waiting for further suggestions.
Thanks in advance
Dimitar
~Best
Dimitar Gamishev said:When Random HWGen is disabled board boots and hangs at same place.
Do you mean "Waiting for root device /dev/mmcblk0p2..." ?
Dimitar Gamishev said:I made some tests with 3.11.0 and board boots fine.
Are you using the same device tree files in both cases?
What exactly are the differences between the kernel configurations?
Best regards,
Miroslav
Hi Miroslav,
sorry for delay.
There is no significant difference between configs. I think the problem is in VDD regulator, in our design we do not use PMU. I think omap_hsmmc fails to load because of this :
[ 2.114389] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[ 2.135340] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
Is there a way to disable PMU at all ?
~Best