This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H.264 decoder fails to run with HEVC encoder



Hi,

In my transcoder I can't run multicore H.264 decoder (2 or 4 cores mode) with HEVC encoder simultaneously.

All works good when:

1) H.264 decoder runs in single-core mode with HEVC

or

2) H.264 decoder's process calls are not executed simultaneously with HEVC process calls.

or

3) When I use H.264 decoder with other than HEVC encoders (i.e. multicore or singlecore H.264 encoder).

But when I run H.264 multicore decoder simultaneously with singlecore or multicore HEVC encoder it hangs.
 HEVC encoder runs on core 4, H.264 decoder runs on cores 0-3.

Have you ever run transcoding: H.264 decoder with HEVC encoder?

I use H.264 decoder 01.01.04.00 and 01.01.04.02.

I use HEVC encoder from MCSDK Video 02.02.00.42 and 02.02.00.41

Regards,

Andrey Lisnevich