Hi,
Does anyone know where I can find the schematics for the Rev C board? The one I got from TI's store is a rev C board. But on the ti's website
http://focus.ti.com/dsp/docs/dspcontent.tsp?contentId=62032
I can only find the related info for Rev B.
Aside from the different expansion connector (Rev C has a 60 pin connector, which Rev B only has 40 pins), is there anything else different? The reason we need the updated schematic is because we are using the usb's schematics as a reference.
Also, for the pin defination of the expanstion connector in Rev C, we are assuming the document "C5505 USB Stick Edge Connector Details" at
http://support.spectrumdigital.com/boards/usbstk5505/revb/
Is accurate on the mapping between Rev C and Rev B.
It would be good if someone can confirm this.
Thanks
Shen