This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

kernel boot failure

Guru 20755 points

Hello,

I am working on new custom board, and the kernel is stuck on boot as following:


Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (ubuntu@ubuntu-laptop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #28 Thu Aug 7 ..........
omap_mux_init: Add partition: #1: core, flags: 4
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS


There are no more printing. 

I see that it is stuck somewhere here:

init_idle_bootup_task(current);
preempt_enable_no_resched();
schedule();
<<-- never gets here !!!
preempt_disable();

I see similar problem in the following uresolved thread:
http://e2e.ti.com/support/arm/sitara_arm/f/791/p/270550/1273216.aspx#1273216

Are there any solution ?

I would appreciate any guidance.

Thanks,

Ran