This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

aplay error



Hi, I use RDK4.0.0.3 on DM8168, When input the follow command on console,

aplay -D hw:0,1 -r 44100 -c 2 -f cd test.wav

Then the console echo:

Playing WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

 aplay: pcm_write:1710: write error: Input/output error

How do i solve this ?

Thanks.