This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two DM8168 four channel display

One DM8168 can output only two independent channels display, Now I want to increase the  decoding performance and ouput four  independent channels display, so I cascade two DM8168 chips for  four  independent channels display.

There are some problems for me to do it:

1. Could DM8168 chips cascade output four independent channels display? 

2. If the DM8168 chips cascade output four independent channels display, How could I connect the two DM8168 chips? Use PCI-E?

3. Does two DM8168 chips need their own independent systems, including the Linux Kernel, application and etc?