Other Parts Discussed in Thread: SPRC090
how to do the programming on c6713 for speech recognition???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SPRC090
how to do the programming on c6713 for speech recognition???
Hi,
Thanks for your post.
I don't think, there are example projects available for speech recognition, but there is minimal audio example project through AIC23 codec using board support library and I would recommend where you can start from this:
http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5#Importing_sample_projects
From the above wiki, you can download the audio minimal project zip file from the below:
http://processors.wiki.ti.com/index.php/File:C6713_audio_minimal.zip
Also, you have CSL package available for C6713 devices which you can download from the below wiki:
http://processors.wiki.ti.com/index.php/Chip_support_library#C62x.2C_C671x.2C_C641x.2C_DM64x_Devices
and you can download the same CSL package available below:
http://www.ti.com/tool/sprc090
Alternatively, i would recommend you to attend a live tms320C6x1x DSP integration workshop as below:
http://processors.wiki.ti.com/index.php/TMS320C6x1x_DSP_Integration_Workshop
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------