Dear All,
In our customized board we are having two DSP(C6678) processor. The switch setting is kept in NO BOOT Mode. We have customized the GEL File according to the Board hardware components. After Successful Initialization of GEL, I have accessed the Reserved address region 0x02620008 through the memory browser. The value returned is
For DSP 1 - 0x08014013;
For DSP 2 - 0x0901500B;
For EVM - 0x01013005;
Questions:
1. What the value actually specifying or Intimating?
2. Why there is a difference in the value of the Reserved address?
3. If suppose we are using 5 DSP Processor in a single board and the value of 0x02620008 address section will vary for every processor ?
It is very urgent can any one clarify the doubt?
Thanks in advance.
Regards,
Avinash N